Blog : Smart Connections

  • Office & Enterprise

    Mike Holmes Jan 5, 2022

    Do Smart Buildings still have a future?

    The past two years has seen a major shift worldwide in the workplace. Many employees suddenly found themselves having to work from home, leaving a skeleton staff to man mostly empty offices. What are the consequences for Smart Buildings following this recent wave of furloughing and teleworking? Is the Smart Office doomed to disappear or does it still have a bright future ahead as many believed not so long ago?

  • Office & Enterprise

    Jan Middeldorf Dec 9, 2021

    What will new WAPs and networked devices mean for the LAN?

    How Fibre To the Office supports next-generation Wi-Fi and LAN device requirements

  • Office & Enterprise

    Alexandra Nacken Nov 23, 2021

    All you need to know about future-ready LANs

    Which developments are affecting local area networks?

  • Telecom

    Arnaud Caudreliez Oct 4, 2021

    ISO 45001 certification – why does it matter?

    Between September 2020 and January 2021, three ISO 45001 audits were carried out at Nexans Interface telecom systems plant in Vrigne-aux-Bois, France. These audits looked at documentation, management processes, and finally a field evaluation. Only two minor deviations were identified, and, after corrective actions put in place, Nexans Interface became ISO 45001 certified. But what is ISO 45001 and why does it matter?

  • Telecom

    Julien Loterie Sep 17, 2021

    Taking micro-blown fibre cable to the next level

    There are different ways you can install micro-fibre cables outdoors in tubes. The preferred option is by blowing. Blowing or jetting offers numerous advantages and is widely adopted by operators worldwide to deploy high speed bandwidth to consumers.